Hi all,
I want to run DDR Stress Tester on the cutomer original iMX53 board.
However, I need to change to UART-4 port from UART-1 port.
The UART4 port is below.
-TXD CSI0_DATA12/ALT2
-RXD CSI0_DATA13/ALT3
Which part of source code do I change ?
*I have already got a source code of the DDR_Stress_Tester_for_mx51mx53_V002 from FSL local FAE.
Ko-hey
已解决! 转到解答。
Hi ko-hey
one can add codes to function debug_uart_iomux() in hardware.c
alternatively one can add uart4 iomux settings in *.inc file like
..\DDR_Stress_Tester_for_mx51mx53_V002\binary\MX53_TO2_DDR3_LCB.inc
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ko-hey
one can add codes to function debug_uart_iomux() in hardware.c
alternatively one can add uart4 iomux settings in *.inc file like
..\DDR_Stress_Tester_for_mx51mx53_V002\binary\MX53_TO2_DDR3_LCB.inc
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------