Model Voltage error when simulating i.MX8 QM LPDDR4 interface with Hyperlynx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Model Voltage error when simulating i.MX8 QM LPDDR4 interface with Hyperlynx

1,312 Views
RichG
Contributor III

Hello. I have a design where I'm using the same LPDDR4 chips as the NXP eval board and in fact I have the same layout (pulled it in from the ODB++ files). It should work but I wanted to run a simulation to check. The models I'm using are:

i.MX8QM: imx8qm_29x29_rev1_25.ibs

MT53E768M32D4DT LPDDR4: z1am_200b-qdp_x32.ebd

The micron model within that ebd file is set to z1am_0p6V_st.ibs

When I set up the DDRx Batch Mode test in Hyperlynx, I get the following error:

There are nets with IBIS model voltage range compatibility issues:
Net(s): DDR_CH0_DM0..3, DDR_CH0_DQ0..31, DDR_CH1_DM0..3, DDR_CH1_DQ0..31
IBIS File: C:\Hyp\ADCMK5\Models\IMX8QM-IBIS\imx8qm_29x29_rev1_25.ibs
Selector/Model, Voltage: PDDRIO_PAD_DATA / DWC_D5MPL4_40 1.1V
Device(s): U1
IBIS File: C:\Hyp\ADCMK5\Models\MT53E768M32D4DT-053_ibis\z1am_0p6v_wt.ibs
Selector/Model, Voltage: DQ / DQ_PD40_ODT40_VOH50_4266 0.6V
Device(s): U0_EBD-U4, U2_EBD-U4

Am I trying to use the wrong models?

Thanks so much!

Rich

0 Kudos
Reply
0 Replies