Missing bluetooth (UART4) on Solidrun Hummingboard Pulse (iMX8)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Missing bluetooth (UART4) on Solidrun Hummingboard Pulse (iMX8)

1,457 Views
garyg
Contributor I

According to Solidrun HB spec they used UBLOX BT module that connects to UART4. I can see the /dev/ttymxc3 but failed to see bluetoothctl controller.

Is there any driver that I need to install to expose it on user space? E.g. hciconfig hci0

0 Kudos
Reply
1 Reply

1,408 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hello Gary,

I strongly suggest that you submit your question on the Solid Run Forum,

http://forum.solid-run.com/ 

Since the BSP that they are using it is different from the NXP official release for the  i.MX8M EVK board.

0 Kudos
Reply