Minimal schematic for MIMXRT1062DVL6A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Minimal schematic for MIMXRT1062DVL6A?

2,050 Views
Elmi77
Contributor III

Hi,

is there a minimal schematic for the iMXRT1062 available somewhere? Means no perihperals, only these components that are required to start it successfully at full speed?

Thanks!

 

0 Kudos
Reply
1 Reply

2,033 Views
art
NXP Employee
NXP Employee

There is no dedicated "minimal" schematic available for the i.MX RT1062 processor. However, it can easily be defined.

Please refer to the i.MX RT1062 EVK board schematic, available here:

https://www.nxp.com/webapp/Download?colCode=MIMXRT1060-EVK-DESIGNFILE-A3

The minimum operating environment requires the power supply as shown on the Sheet 4 of the schematic above, at least one of possible boot media devices out of shown on the Sheet 11, boot configuration resistor network as shown on the Sheet 16 and the USB OTG port to program the device in the Serial Downloader mode as shown on the Sheet 7.

Best Regards,
Artur