Microcode SW error detected. Restarting 0x2000000.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Microcode SW error detected. Restarting 0x2000000.

Jump to solution
7,001 Views
toniehuang
Contributor II

Hi,

I am trying to port Intel Centrino-N 135 wifi module into iMx6q. (Android ICS version, code base is R13.4)

For figuring out what issues are I met, here are my procedures :

1. insmod cfg80211.ko

2. insmod mac80211.ko

3. insmod iwlan.ko debug=0x43ffff

Till now, those output messages are quite ok.

Then I started the wpa_supplicant, then those messages are coming :

start wpa_supplicant

ieee80211 phy0: U iwlagn_mac_start enter

ieee80211 phy0: U iwl_prep_station Add STA to driver ID 15: ff:ff:ff:ff:ff:ff

ieee80211 phy0: U iwl_prep_station Add STA to driver ID 14: ff:ff:ff:ff:ff:ff

ieee80211 phy0: U iwl_prepare_card_hw iwl_prepare_card_hw enter

ieee80211 phy0: U iwl_set_hw_ready hardware ready

ieee80211 phy0: U iwl_apm_init Init card's basic functions

ieee80211 phy0: U iwl_apm_init L1 Disabled; Enabling L0S

ieee80211 phy0: U iwlagn_load_section INST uCode section being loaded...

ieee80211 phy0: U iwlagn_load_section DATA uCode section being loaded...

ieee80211 phy0: I iwlagn_alive_fn Alive ucode status 0x00000001 revision 0x1 0x9

ieee80211 phy0: U iwlcore_verify_inst_sparse ucode inst image size is 139180

ieee80211 phy0: U iwl_verify_ucode uCode is good in inst SRAM

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 0 on FIFO 3

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 1 on FIFO 2

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 2 on FIFO 1

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 3 on FIFO 0

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 4 on FIFO 0

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 5 on FIFO 4

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 6 on FIFO 2

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 7 on FIFO 5

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 8 on FIFO 4

ieee80211 phy0: U iwlagn_tx_queue_set_status Activate AC/CMD Queue 9 on FIFO 7

ieee80211 phy0: U iwl_send_cmd_sync Attempting to send sync command COEX_PRIORITY_TABLE_CMD

ieee80211 phy0: U iwl_send_cmd_sync Setting HCMD_ACTIVE for command COEX_PRIORITY_TABLE_CMD

ieee80211 phy0: U iwl_enqueue_hcmd Sending command COEX_PRIORITY_TABLE_CMD (#5a), seq: 0x0900, 72 bytes at 0[0]:9

ieee80211 phy0: I iwl_tx_cmd_complete Clearing HCMD_ACTIVE for command COEX_PRIORITY_TABLE_CMD

iwlagn 0000:01:00.0: Microcode SW error detected.  Restarting 0x2000000.

iwlagn 0000:01:00.0: Loaded firmware version: 18.168.6.1

iwlagn 0000:01:00.0: Start IWL Error Log Dump:

iwlagn 0000:01:00.0: Status: 0x00040224, count: 6

iwlagn 0000:01:00.0: 0x000019B4 | ADVANCED_SYSASSERT

iwlagn 0000:01:00.0: 0x00014D38 | uPc

iwlagn 0000:01:00.0: 0x00014D2A | branchlink1

iwlagn 0000:01:00.0: 0x00014D2A | branchlink2

iwlagn 0000:01:00.0: 0x0000CDCE | interruptlink1

iwlagn 0000:01:00.0: 0x00000000 | interruptlink2

iwlagn 0000:01:00.0: 0x0000021F | data1

iwlagn 0000:01:00.0: 0x00000171 | data2

iwlagn 0000:01:00.0: 0x00000171 | line

iwlagn 0000:01:00.0: 0x004071C0 | beacon time

iwlagn 0000:01:00.0: 0x0002AE40 | tsf low

iwlagn 0000:01:00.0: 0x00000000 | tsf hi

iwlagn 0000:01:00.0: 0x00000000 | time gp1

iwlagn 0000:01:00.0: 0x0002AE44 | time gp2

iwlagn 0000:01:00.0: 0x00000000 | time gp3

iwlagn 0000:01:00.0: 0x754312A8 | uCode version

iwlagn 0000:01:00.0: 0x00000120 | hw version

iwlagn 0000:01:00.0: 0x00C80300 | board version

iwlagn 0000:01:00.0: 0x0900005A | hcmd

iwlagn 0000:01:00.0: CSR values:

iwlagn 0000:01:00.0: (2nd byte of CSR_INT_COALESCING is CSR_INT_PERIODIC_REG)

iwlagn 0000:01:00.0:        CSR_HW_IF_CONFIG_REG: 0X00c80300

iwlagn 0000:01:00.0:          CSR_INT_COALESCING: 0X0000ff40

iwlagn 0000:01:00.0:                     CSR_INT: 0X10000000

iwlagn 0000:01:00.0:                CSR_INT_MASK: 0X00000000

iwlagn 0000:01:00.0:           CSR_FH_INT_STATUS: 0X00000000

iwlagn 0000:01:00.0:                 CSR_GPIO_IN: 0X00000000

iwlagn 0000:01:00.0:                   CSR_RESET: 0X00000000

iwlagn 0000:01:00.0:                CSR_GP_CNTRL: 0X080403c5

iwlagn 0000:01:00.0:                  CSR_HW_REV: 0X00000120

iwlagn 0000:01:00.0:              CSR_EEPROM_REG: 0X45180ffd

iwlagn 0000:01:00.0:               CSR_EEPROM_GP: 0X90000801

iwlagn 0000:01:00.0:              CSR_OTP_GP_REG: 0X00030001

iwlagn 0000:01:00.0:                 CSR_GIO_REG: 0X00080044

iwlagn 0000:01:00.0:            CSR_GP_UCODE_REG: 0X0000001e

iwlagn 0000:01:00.0:           CSR_GP_DRIVER_REG: 0X00000000

iwlagn 0000:01:00.0:           CSR_UCODE_DRV_GP1: 0X00000000

iwlagn 0000:01:00.0:           CSR_UCODE_DRV_GP2: 0X00000000

iwlagn 0000:01:00.0:                 CSR_LED_REG: 0X00000018

iwlagn 0000:01:00.0:        CSR_DRAM_INT_TBL_REG: 0X00000000

iwlagn 0000:01:00.0:        CSR_GIO_CHICKEN_BITS: 0X29800200

iwlagn 0000:01:00.0:             CSR_ANA_PLL_CFG: 0X00000000

iwlagn 0000:01:00.0:           CSR_HW_REV_WA_REG: 0X0001001a

iwlagn 0000:01:00.0:        CSR_DBG_HPET_MEM_REG: 0Xffff0000

iwlagn 0000:01:00.0: FH register values:

iwlagn 0000:01:00.0:         FH_RSCSR_CHNL0_STTS_WPTR_REG: 0X0279d100

iwlagn 0000:01:00.0:        FH_RSCSR_CHNL0_RBDCB_BASE_REG: 0X0027e2d0

iwlagn 0000:01:00.0:                  FH_RSCSR_CHNL0_WPTR: 0X00000000

iwlagn 0000:01:00.0:         FH_MEM_RCSR_CHNL0_CONFIG_REG: 0X80819104

iwlagn 0000:01:00.0:          FH_MEM_RSSR_SHARED_CTRL_REG: 0X000000fc

iwlagn 0000:01:00.0:            FH_MEM_RSSR_RX_STATUS_REG: 0X07030000

iwlagn 0000:01:00.0:    FH_MEM_RSSR_RX_ENABLE_ERR_IRQ2DRV: 0X00000000

iwlagn 0000:01:00.0:                FH_TSSR_TX_STATUS_REG: 0X07ff0001

iwlagn 0000:01:00.0:                 FH_TSSR_TX_ERROR_REG: 0X00000000

iwlagn 0000:01:00.0: Start IWL Event Log Dump: display last 20 entries

iwlagn 0000:01:00.0: EVT_LOGT:0000026983:0x000000ff:1100

iwlagn 0000:01:00.0: EVT_LOGT:0000026984:0x000000ff:1100

iwlagn 0000:01:00.0: EVT_LOGT:0000026985:0x000000ff:1100

iwlagn 0000:01:00.0: EVT_LOGT:0000026985:0x000000ff:1100

iwlagn 0000:01:00.0: EVT_LOGT:0000026986:0x000000ff:1100

iwlagn 0000:01:00.0: EVT_LOGT:0000174346:0x0900005a:0401

iwlagn 0000:01:00.0: EVT_LOGT:0000174347:0x0900005a:1512

iwlagn 0000:01:00.0: EVT_LOGT:0000174457:0x00000003:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174457:0x00000003:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174458:0x00000000:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174460:0x00000004:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174461:0x00000003:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174464:0x00000001:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174464:0x00000000:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174465:0x00000001:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174466:0x00000001:1211

iwlagn 0000:01:00.0: EVT_LOGT:0000174466:0xcafe0001:1214

iwlagn 0000:01:00.0: EVT_LOGT:0000175229:0x0002ac7d:1110

iwlagn 0000:01:00.0: EVT_LOGT:0000175681:0x0000021f:1132

iwlagn 0000:01:00.0: EVT_LOGT:0000175691:0x00000000:0125

ieee80211 phy0: U iwl_send_cmd_sync Attempting to send sync command REPLY_PHY_CALIBRATION_CMD

ieee80211 phy0: U iwl_send_cmd_sync Setting HCMD_ACTIVE for command REPLY_PHY_CALIBRATION_CMD

ieee80211 phy0: U iwl_enqueue_hcmd Sending command REPLY_PHY_CALIBRATION_CMD (#b0), seq: 0x0901, 12 bytes at 1[1]:9

iwlagn 0000:01:00.0: Error sending REPLY_PHY_CALIBRATION_CMD: time out after 500ms.

ieee80211 phy0: U iwl_send_cmd_sync Clearing HCMD_ACTIVE for command REPLY_PHY_CALIBRATION_CMD

iwlagn 0000:01:00.0: Error -110 iteration 0

iwlagn 0000:01:00.0: Could not complete ALIVE transition: -110

ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state

ieee80211 phy0: U iwl_apm_stop_master stop master

iwlagn 0000:01:00.0: Failed to run INIT ucode: -110

ieee80211 phy0: U __iwl_down iwlagn is going down

ieee80211 phy0: U iwl_scan_cancel_timeout Scan cancel timeout

ieee80211 phy0: U iwl_do_scan_abort Not performing scan to abort

ieee80211 phy0: U iwl_clear_ucode_stations Clearing ucode stations in driver

ieee80211 phy0: U iwl_clear_ucode_stations No active stations found to be cleared

ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state

ieee80211 phy0: U iwl_apm_stop_master stop master

iwlagn 0000:01:00.0: Unable to initialize device.

ieee80211 phy0: U __iwl_down iwlagn is going down

ieee80211 phy0: U iwl_scan_cancel_timeout Scan cancel timeout

ieee80211 phy0: U iwl_do_scan_abort Not performing scan to abort

ieee80211 phy0: U iwl_clear_ucode_stations Clearing ucode stations in driver

ieee80211 phy0: U iwl_clear_ucode_stations No active stations found to be cleared

ieee80211 phy0: U iwl_apm_stop Stop card, put in low power state

ieee80211 phy0: U iwl_apm_stop_master stop master

ieee80211 phy0: Hardware restart was requested

ieee80211 phy0: U iwlagn_configure_filter Enter: changed: 0x0, total: 0x80000000

root@android:/system/lib/modules #

root@android:/system/lib/modules # logcat

--------- beginning of /dev/log/main

D/wpa_supplicant( 2917): wpa_supplicant v0.8.x

D/wpa_supplicant( 2917): Add randomness: count=1 entropy=0

D/wpa_supplicant( 2917): random: Added entropy from /data/misc/wifi/entropy.bin (own_pool_ready=2)

D/wpa_supplicant( 2917): random: Trying to read entropy from /dev/random

D/wpa_supplicant( 2917): Get randomness: len=20 entropy=1

D/wpa_supplicant( 2917): random: Updated entropy file /data/misc/wifi/entropy.bin (own_pool_ready=2)

D/wpa_supplicant( 2917): Initializing interface 'wlan0' conf '/system/etc/wifi/wpa_supplicant.conf' driver 'nl80211' ctrl_interface 'N/A' bridge 'N/A'

D/wpa_supplicant( 2917): Configuration file '/system/etc/wifi/wpa_supplicant.conf' -> '/system/etc/wifi/wpa_supplicant.conf'

D/wpa_supplicant( 2917): Reading configuration file '/system/etc/wifi/wpa_supplicant.conf'

D/wpa_supplicant( 2917): update_config=1

D/wpa_supplicant( 2917): ctrl_interface='DIR=/data/system/wpa_supplicant GROUP=wifi'

D/wpa_supplicant( 2917): ap_scan=0

D/wpa_supplicant( 2917): Line: 8 - start of a new network block

D/wpa_supplicant( 2917): key_mgmt: 0x4

D/wpa_supplicant( 2917): Priority group 0

D/wpa_supplicant( 2917):    id=0 ssid=''

D/wpa_supplicant( 2917): nl80211: interface wlan0 in phy phy0

I/wpa_supplicant( 2917): rfkill: Cannot open RFKILL control device

D/wpa_supplicant( 2917): nl80211: RFKILL status not available

E/wpa_supplicant( 2917): Could not set interface wlan0 flags: Connection timed out

E/wpa_supplicant( 2917): nl80211: Could not set interface 'wlan0' UP

E/wpa_supplicant( 2917): wlan0: Failed to initialize driver interface

D/wpa_supplicant( 2917): Failed to add interface wlan0

D/wpa_supplicant( 2917): Get randomness: len=20 entropy=0

D/wpa_supplicant( 2917): random: Updated entropy file /data/misc/wifi/entropy.bin (own_pool_ready=2)

Can anyone give me hint or suggestion ?

Regards,

Tonie

Labels (2)
1 Solution
6,285 Views
israelpz
Senior Contributor I

Hi Tony,

Looking at detail on the error dump i could say the following:

Even your are using a intel PCI express. Internally they use a CSR wifi ip.

The setup registers which could be configured at boot time on CSR chips are call PSKEYS like

"CSR_HW_IF_CONFIG_REG", "CSR_UCODE_DRV_GP2" , etc.

Those registers are documented in NDA technical document provided by CSR.

The problem here is somehow a binary with the PSKEYS is loaded but that cause a failure in

the communication with the CSR wifi module (that is very similar to a issue Bluetooth module).

The only way to solved it is not loading that binary(firmware bin) or ask intel to provide a tested/working firmware binary.

Regards,

-Israel.

View solution in original post

0 Kudos
Reply
8 Replies
6,285 Views
toniehuang
Contributor II

Hi,

I've fixed this issue by other way.

As we know that the driver for Intel wifi modules came from backports-3.xxxx... (or compat-wireless-xxxx)

What I did was :

I download many different version of intel wirelss driver and try to port into my board.

And I found one version of these can work without modifying may code in driver.

This is just what I did and how I fix my issue.

Thanks.

0 Kudos
Reply
6,286 Views
israelpz
Senior Contributor I

Hi Tony,

Looking at detail on the error dump i could say the following:

Even your are using a intel PCI express. Internally they use a CSR wifi ip.

The setup registers which could be configured at boot time on CSR chips are call PSKEYS like

"CSR_HW_IF_CONFIG_REG", "CSR_UCODE_DRV_GP2" , etc.

Those registers are documented in NDA technical document provided by CSR.

The problem here is somehow a binary with the PSKEYS is loaded but that cause a failure in

the communication with the CSR wifi module (that is very similar to a issue Bluetooth module).

The only way to solved it is not loading that binary(firmware bin) or ask intel to provide a tested/working firmware binary.

Regards,

-Israel.

0 Kudos
Reply
6,285 Views
toniehuang
Contributor II

Hi, Israel,

Thanks for your information.

I will try to follow your suggestion and tell if I have any result.

Regards,

Tonie

0 Kudos
Reply
6,285 Views
mralmond
Contributor II

Hi, I'm having the same issue using a pcie card with Intel 6235 on an i.mx6 board with kernel 3.0.35.

Have you been able to solve this problem?

0 Kudos
Reply
6,285 Views
israelpz
Senior Contributor I

Hi,

Seem to be a problem with the physical layer.

Are you using a PCI express module? Or is USB?

I ask because similar errors also appear on Bluetooth layer when the buadrate, parity or link layer are not setup

properly to the ones stored in the chip firmware then it will start to generate timeouts and also frame errors.

Do you have that information for that wifi module?

Regards,

-Israel

6,285 Views
toniehuang
Contributor II

Hi, Israel,

Sorry for lately response.

What I used is PCI express modules.

And I didn't have any further information about that wifi module. (Intel doesn't release any doc to us)

All I have is those file from the opensource of Intel wifi module.

Regards,

Tonie

0 Kudos
Reply
6,285 Views
imxcommunitysco
Senior Contributor II

Tonie, did Israel answer your question. If yes, please click Correct Answer button so that we can close the DI.

Regards,

Yixing,

0 Kudos
Reply
6,285 Views
karina_valencia
NXP Apps Support
NXP Apps Support

Hi,

Seem to be a problem with the physical layer.

Are you using a PCI express module? Or is USB?

I ask because similar errors also appear on Bluetooth layer when the buadrate, parity or link layer are not setup

properly to the ones stored in the chip firmware then it will start to generate timeouts and also frame errors.

Do you have that information for that wifi module?

Regards,

-Israel

0 Kudos
Reply