Mfgtool flashing issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mfgtool flashing issue

Jump to solution
1,917 Views
manjunathjoshi
Contributor V

Hello all,

I am seeing a tar error at the very end of a flash which i am attaching. Can anybody guess what's the exact issue?

Has anybody got similar issue ? Please let me know as soon as possible.

Regards,

Manju

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,712 Views
manjunathjoshi
Contributor V

Hello All,

This issue was solved when i renamed rootfs.tar.bz2 to rootfs.tar.

This is a work around but surely worked for me.

Regards,

Manju

View solution in original post

0 Kudos
Reply
3 Replies
1,712 Views
b36401
NXP Employee
NXP Employee

The error itself (invalid tar magic) means that tar does not find archive signature.

It may be caused with damaged image.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,712 Views
manjunathjoshi
Contributor V

Hello victor,

The same image is untarred in many other boards. That's the tricky part.

I want to know when such error might occur? Not one instance of it.

Regards,

Manju

0 Kudos
Reply
1,713 Views
manjunathjoshi
Contributor V

Hello All,

This issue was solved when i renamed rootfs.tar.bz2 to rootfs.tar.

This is a work around but surely worked for me.

Regards,

Manju

0 Kudos
Reply