Mfgtool Format Disc pop-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mfgtool Format Disc pop-up

1,486 Views
ashokkumarredd1
Contributor I

Hi

when we flash SW using Mfgtool "format disc popup" will appear (discarding  popup as it does not affect any functionality).

Is there any way we can fix in OS side to disable popup  as Mfgtool uses UTP protocol to transfer images i am not sure fixing that in OS side may have side effects

Is there any proven solution available?

Regards,

Ashok

Labels (1)
0 Kudos
Reply
1 Reply

1,374 Views
art
NXP Employee
NXP Employee

Actually, this is not the MFGtool pop-up but the OS pop-up. It occurs at the moment when target board switches from emulating USB HID device to USB Mass-storage device. Typically, it occurs on slowly-running host OSes. Try to do it on a faster machine :-)


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply