Hi All,
I just received a MCIMX6ULL-EVK this week. I tried to download image using MfgTool2 with L4.9.88_2.0.0 iMX6,7 BSP. But it show error message below when I downloading the image.
U-Boot 2017.03-imx_v2017.03_4.9.88_2.0.0_ga+gb76bb1b (May 01 2018 - 15:03:05 -05 00)
CPU: Freescale i.MX6ULL rev1.0 at 396 MHz
Reset cause: POR
Model: Freescale i.MX6 ULL DDR3 ARM2 Board
Board: MX6ULL 14X14 DDR3 ARM2
DRAM: 1 GiB
ERROR: read error from device: bef4a9a8 register: 0x0!
at /home/bamboo/build/4.9.X-2.X/fsl-imx-xwayland/temp_build_dir/build_fsl-imx-xw ayland/tmp/work/imx6ull14x14ddr3arm2-poky-linux-gnueabi/u-boot-imx/2017.03-r0/gi t/drivers/power/pmic/pfuze100.c:46/pfuze100_read()
Not supported, id=11
initcall sequence bffa8920 failed at call 878042d4 (err=-22)
### ERROR ### Please RESET the board ###
Kindly need your help on this?
Thanks.
Regards,
XH Low
解決済! 解決策の投稿を見る。
Hi Igor,
We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.
Thanks.
Regards,
XH Low
Hi Igor,
We able to download the image. Just double click one of the desired .vbs script to run the mfgtool.
Thanks.
Regards,
XH Low
Hi XH Low
from log it is not MCIMX6ULL-EVK but "MX6ULL 14X14 DDR3 ARM2" and it has
different uboot image:
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
May I know where to get this u-boot image?
Thanks.
Regards,
XH Low
Hi XH Low
please try
Best regards
igor