Maximum display resolution and frame rate of i.MX51

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum display resolution and frame rate of i.MX51

768 次查看
admin
Specialist II

Saved FAQ from Freescale.com for information only:

Topic: Display, IPU, LCD

 

Question.  What is maximum display resolution and frame rate of i.MX51 ?

 

Answer.  Maximum display resolution : 4096x4048 pixels; Maximum pixel rate: 110 MP/sec

 

The maximum refresh rate is: 110M / (W * H * B), where

- W*H is the display resolution

- B is a factor >1 reflecting blanking overhead,

e.g. as specified by

VESA, CEA-861-D, etc.

 

 Related Products:

 i.MX Applications Processors > i.MX51 Processors > i.MX512, i.MX513, i.MX514, i.MX515, i.MX516

标记 (1)
0 项奖励
回复
0 回复数