Maximum RAM size i.MX 8M can support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Maximum RAM size i.MX 8M can support

跳至解决方案
5,432 次查看
shuodo
Contributor II

Hi,

I would like to find out the maximum RAM size i.MX 8M can support.

I read the reference manual of IMX 8M. Section 2.1.2 A53 memory map, it says DDR memory size is 1 + 3 = 4GB:

A53-DDR-MEM.png

 

However, in section 9.1.1.1, DRAM interface summary says max up to 8GB of memory:

MAX-8GB.png

 

Which one is correct?

Or both are correct? They could be different things: one for DDR memory map size, the other one is for the max DDR size that DDR interface can support? If this is true, how could it handle map 8GB DDR into 4GB of memory space?

 

Best regards.

标记 (2)
0 项奖励
回复
1 解答
5,402 次查看
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

在原帖中查看解决方案

0 项奖励
回复
3 回复数
5,416 次查看
joanxie
NXP TechSupport
NXP TechSupport

do you mean imx8mm, imx8mn, imx8mq or imx8mp?

0 项奖励
回复
5,414 次查看
shuodo
Contributor II
0 项奖励
回复
5,403 次查看
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

0 项奖励
回复