Maximum RAM size i.MX 8M can support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Maximum RAM size i.MX 8M can support

ソリューションへジャンプ
5,391件の閲覧回数
shuodo
Contributor II

Hi,

I would like to find out the maximum RAM size i.MX 8M can support.

I read the reference manual of IMX 8M. Section 2.1.2 A53 memory map, it says DDR memory size is 1 + 3 = 4GB:

A53-DDR-MEM.png

 

However, in section 9.1.1.1, DRAM interface summary says max up to 8GB of memory:

MAX-8GB.png

 

Which one is correct?

Or both are correct? They could be different things: one for DDR memory map size, the other one is for the max DDR size that DDR interface can support? If this is true, how could it handle map 8GB DDR into 4GB of memory space?

 

Best regards.

タグ(2)
0 件の賞賛
返信
1 解決策
5,361件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
5,375件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

do you mean imx8mm, imx8mn, imx8mq or imx8mp?

0 件の賞賛
返信
5,373件の閲覧回数
shuodo
Contributor II
0 件の賞賛
返信
5,362件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for imx8mq, the max density is 4G

0 件の賞賛
返信