MacOS imx_usb "claim interface failed" error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MacOS imx_usb "claim interface failed" error

2,970 Views
bmoon
Contributor I

I'm trying to use imx_usb on a Mac. I observe the following output when I invoke "sudo ./imx_usb":

config file <.//imx_usb.conf>

vid=0x066f pid=0x3780 file_name=mx23_usb_work.conf

vid=0x15a2 pid=0x004f file_name=mx28_usb_work.conf

vid=0x15a2 pid=0x0052 file_name=mx50_usb_work.conf

vid=0x15a2 pid=0x0054 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0061 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0063 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0071 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x007d file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0080 file_name=mx6ull_usb_work.conf

vid=0x1fc9 pid=0x0128 file_name=mx6_usb_work.conf

vid=0x15a2 pid=0x0076 file_name=mx7_usb_work.conf

vid=0x1fc9 pid=0x0126 file_name=mx7ulp_usb_work.conf

vid=0x15a2 pid=0x0041 file_name=mx51_usb_work.conf

vid=0x15a2 pid=0x004e file_name=mx53_usb_work.conf

vid=0x15a2 pid=0x006a file_name=vybrid_usb_work.conf

vid=0x066f pid=0x37ff file_name=linux_gadget.conf

vid=0x1b67 pid=0x4fff file_name=mx6_usb_sdp_spl.conf

vid=0x0525 pid=0xb4a4 file_name=mx6_usb_sdp_spl.conf

vid=0x1fc9 pid=0x012b file_name=mx8mq_usb_work.conf

vid=0x1fc9 pid=0x0134 file_name=mx8mm_usb_work.conf

vid=0x1fc9 pid=0x013e file_name=mx8mn_usb_work.conf

vid=0x3016 pid=0x1001 file_name=mx8m_usb_sdp_spl.conf

config file <.//mx6_usb_work.conf>

parse .//mx6_usb_work.conf

Trying to open device vid=0x15a2 pid=0x0061

claim interface failed

The last line (highlighted in bold) above is the subject of my question. Does anyone know how to correct this "claim interface failed" problem on a Mac with High Sierra (10.13.6)?

Labels (1)
0 Kudos
Reply
3 Replies

2,890 Views
bmoon
Contributor I

Thank you for the response, Weidong. I don't actually know how to determine which kernel extension got associated with the iMX usb client. So, I don't know if the problem I am encountering matches your description or not.

I worked around it by installing an ubuntu VM on my Mac, which works fine.

Thank you for your help.

-Brian

0 Kudos
Reply

2,890 Views
weidong_sun
NXP TechSupport
NXP TechSupport

That's great!

Anyway it finally works fine!

Have a nice day!

Weidong

0 Kudos
Reply

2,890 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Brian,

    See below, please!

---------------------

Could you check if Mac OS can drive i.MX6 board to be a HID Compliance Device ?

if Mac OS can, the reason why caused the issue you encountered should be for comflicts between HID devices. For example, mouse and keyboard are both HID device, it there are 2 or more HID devices on one USB BUS, the conflict will most likely occurs.

Search the related messages from internet, some people also encontered the same situation as yours.

---------------------

Hope above infromation is helpful for you!

Have a nice day!

B.R,

Weidong

0 Kudos
Reply