MXCFB_WAIT_FOR_VSYNC: timeout 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MXCFB_WAIT_FOR_VSYNC: timeout 0

4,415 Views
janefang
Contributor I

Hello NXP experts,

 

Currently I meet a problem that Android hanged on  MXCFB_WAIT_FOR_VSYNC: timeout 0, which cause LCD no display. When I reboot the sytem, it could work wells. This happens 1 of 3 times. attached is the whole log. Can you please give some suggestions on this issue? thanks.

 

init: Starting service 'zygote'...
init: Starting service 'gatekeeperd'...
init: cannot find '/system/xbin/perfprofd', disabling 'perfprofd'
capability: warning: `daemonsu' uses 32-bit capabilities (legacy support in use)
init: Service 'tfsroot' (pid 176) exited with status 0
EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
healthd: No charger supplies found
healthd: No battery devices found
EXT4-fs (mmcblk0p5): re-mounted. Opts: (null)
init: Untracked pid 260 exited with status 0
ERROR: v4l2 capture: slave not found!
random: nonblocking pool is initialized
imx-ipuv3 2800000.ipu: WARNING: adapt panel end blank lines
init: Starting service 'bootanim'...
cfg80211: World regulatory domain updated:
cfg80211:  DFS Master region: unset
cfg80211:   (start_freq - end_freq @ bandwidth), (max_antenna_gain, max_eirp), (dfs_cac_time)
cfg80211:   (2402000 KHz - 2472000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
cfg80211:   (2457000 KHz - 2482000 KHz @ 20000 KHz), (300 mBi, 2000 mBm), (N/A)
cfg80211:   (2474000 KHz - 2494000 KHz @ 20000 KHz), (300 mBi, 2000 mBm), (N/A)
cfg80211:   (5170000 KHz - 5250000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
cfg80211:   (5735000 KHz - 5835000 KHz @ 40000 KHz), (300 mBi, 2000 mBm), (N/A)
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: timeout when waiting for flip irq
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: timeout when waiting for flip irq
zram: 503 (system_server) Attribute mem_used_total (and others) will be removed. See zram documentation.
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0

Original Attachment has been moved to: session.log.zip

0 Kudos
Reply
1 Reply

2,812 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jane

issue may be caused by ipu reset as described on below links

imx6 android 4.3.1 IPU error when system start 

imx6q mxc_sdc_fb timeout when waiting for flip irq 

usually this happens when using splashscreen, one can look at latest patches on

https://community.freescale.com/docs/DOC-98109

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply