Programming QSPI flash is possible on our customer board with mfg tool an i think, the fuses are set correct (HW_OCOTP_BOOT_CFG0 = 0x10004000, Boot_mode is 00). The QSPI flash was accessed after reboot, but nothing more happens (no console output).
Maybe there´s a problem with the qspi config file (i still use the original qspi-nor-macronix-mx25l51245g-config file). Is a modified config file for the MX66L1G45G available/necessary?
Solved! Go to Solution.
Hi Dieter
unfortunately I am not aware of config file for the MX66L1G45G, just for test one can try to
boot for example in single mode of operation, also check if uboot has support for that flash
Re: [U-Boot] [PATCH] spi: Add support for MX66U51235F, MX66L1G45G and MT25QU02G
attach jtag debugger and dump 0x910400 (ROM uses 0x910000 as starting address),
you should see ivt header here if the qspi access is ok.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
MX66 flash works with MX25 config file. We had a reset problem, flash was held in reset after power up. Now booting from qpi works.
Hi Dieter
unfortunately I am not aware of config file for the MX66L1G45G, just for test one can try to
boot for example in single mode of operation, also check if uboot has support for that flash
Re: [U-Boot] [PATCH] spi: Add support for MX66U51235F, MX66L1G45G and MT25QU02G
attach jtag debugger and dump 0x910400 (ROM uses 0x910000 as starting address),
you should see ivt header here if the qspi access is ok.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------