MX7 - Direct access to Cortex M4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX7 - Direct access to Cortex M4

1,702 Views
demoniacmilk
Contributor IV

Hello everyone,

as I have designed neither USB OTG1 nor an SD card slot into my hardware I cannot boot the MX7D based system with linux it seems.

To test some of the peripherals before doing a hardware redesign Id like to access the M4 on the board and do some memory writes and confirm that NAND/eMMC/RAM are working as intended. Is this possible?
I got access to KEIL. What kind of emulator would I need?

Regards,
Lars

0 Kudos
Reply
1 Reply

1,566 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lars

for direct access to M4 one can use jtag, may be used AN5229

ARM DS-5 Development Studio Debug

https://www.nxp.com/docs/en/application-note/AN5229.pdf 

for keil usually used ulink

ULINK Debug Adapters 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply