MX6Q usb ogt host error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX6Q usb ogt host error

1,666件の閲覧回数
jinjecho
Contributor I

Hi, everybody.

I have a i.mx6 custom board and want to use the usb otg as host.

The board was designed by sabreAI board.

The otg id pin is grounded.

When boot the board by plug the mouse in the otg port, the below messages appear.

usb 1-1: new full speed USB device number 3 using fsl-ehci

usb 1-1: device descriptor read/64, error -71

usb 1-1: device descriptor read/64, error -71

usb 1-1: new full speed USB device number 4 using fsl-ehci

usb 1-1: device not accepting address 4, error -71

usb 1-1: new full speed USB device number 5 using fsl-ehci

usb 1-1: device not accepting address 5, error -71

hub 1-0:1.0: unable to enumerate USB device on port 1

how can i fix it?

Thank you.

ラベル(2)
0 件の賞賛
返信
1 返信

1,382件の閲覧回数
raymondwang
Senior Contributor I

-71 means IO error, Please be sure usb mouse is connected properly.

0 件の賞賛
返信