MX6Q eMMC throughput

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX6Q eMMC throughput

3,736 Views
hankwang
Contributor V

Hi, we tested the eMMC write speed about 10MB/s.  We run the FIO benchmark, the command is fio -filename=/dev/mmcblk3 -direct=1 -iodepth 1 -thread -rw=write -ioengine=psync -bs=4k -size=1g -numjobs=1 -group_reporting -name=test.

As I know, the i.MX6Q didn't support HS200 and HS400. Our eMMC is Micron 8G, the datasheet of Micron has description the max write speed  40MB/s with HS200/400.

We would like know what max write speed is for i.MX6Q?  Thank you.

0 Kudos
Reply
4 Replies

3,725 Views
weidong_sun
NXP TechSupport
NXP TechSupport

For 3.3V IO, below speeds are all supported:

• MMC full speed mode (up to 26 MHz)
• MMC high speed mode (up to 52 MHz)
• MMC DDR mode (52 MHz both edges)

For eMMC4.4 or lower (from internet):

weidong_sun_0-1605761088672.png

the parameters in the list meet those in i.MX6Q reference manual.

 

Have a nice day!

B.R,

weidong

 

0 Kudos
Reply

3,694 Views
hankwang
Contributor V

The max data transfer should be include read and write. The High speed DDR's max data transfer is 104MB/s. We guess this is read speed. Our eMMC datasheet has description this speed is 40MB/s for HS200/400. As I know, the i.MX6Q is not support HS200/400.But eMMC datasheet didn't show DDR speed. So far, we don't know what the ideal write speed should be.  

0 Kudos
Reply

3,731 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi hankwang,

1. IMX6Q uSDHC Data TrThe uSDHC can select the following modes for data transfer:
• SD 1-bit
• SD 4-bit
• MMC 1-bit
• MMC 4-bit
• MMC 8-bit
• Identification Mode (up to 400 kHz)
• MMC full speed mode (up to 26 MHz)
• MMC high speed mode (up to 52 MHz)
• MMC DDR mode (52 MHz both edges)
• SD/SDIO full speed mode (up to 25 MHz)
• SD/SDIO high speed mode (up to 50 MHz)
• SD/SDIO UHS-I mode (up to 208 MHz in SDR mode, up to 50 MHz in DDR mode)

2. VDDIO on Hardware

When you need high-speed mode, the VDDIO voltage of the CPU and EMMC must use 1.8V.

 

Hope this information is helpful to you.

Have a nice day!

B.R,

Weidong

 

0 Kudos
Reply

3,729 Views
hankwang
Contributor V

Hi , 
       Thank you for reply. we would like know which register can select these mode? 
       Do you have write speed data for voltage 1.8V ? Our board voltage is 3.3V for eMMC.
       If the voltage is 3.3V, we can run which mode ?

BRs,

Hank

 

0 Kudos
Reply