MX53 Linux platform successfully launch, Yuanying Tech.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MX53 Linux platform successfully launch, Yuanying Tech.

6,128件の閲覧回数
Oceanblue
Contributor III

        As one technical leading company, in past few year Yuanying Tech always focus on embedded system solution offering, from low end to high end. Our platform including MX25, MX28, MX35 and MX51. From Nov of last year, Yuanying Tech. have started to design MX53 platform based on Linux OS. Now, we have successfully finished this project and launched MX53 Linux OS embedded system platform --- YY- i.MX53L。

 

         i.MX53L is an Linux System Platform based on Linux-2.6.35 kernel, adopt ext2 file system, designed by Yuan-ying Technology. i.MX53L own plentiful peripheral interface, such as USB HOST, USB OTG, TVE Output、DVI、VGA、LVDS、Camera CSI input、SDIO and so on, i.MX53L is widely applied various field, including: HD internet monitor/Automotive Infotainment, industrial computer and thin client machine(cloud computer), MID , Home Media Terminal, V2IP, Factory Automation, HMI design, etc. The dual display feature is the most suitable platform for education equipment. Customer need only focus on the application software design, and largely shorten the time to market cycle.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

6,004件の閲覧回数
KrishnaPavan
Contributor II
Can you provide me the System Boot Flow, the Relevant programs associated with and the concept of NAND Boot flow?
0 件の賞賛
返信

6,004件の閲覧回数
richard0909
Contributor I
Does it support Android?
0 件の賞賛
返信

6,004件の閲覧回数
Oceanblue
Contributor III

690-IMG_0008.jpg

 

         MX53 system board overview from Yuanying Tech.

         Visiting www.yuan-ying.com for the detail. meanwhile, Yuanying Tech. support the mini system board selling alone to speed up customer project design.

0 件の賞賛
返信