MX507: the method to rotate display in Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX507: the method to rotate display in Android

1,167 Views
GraceH
Senior Contributor II

MX507 has no GPU, if rotate display with "setprop ro.sf.hwrotation 90", line shift issue will occur because of software renderer of OpenGL.

We can use the rotate property of EPDC driver to rotate display.

The patch is as below.

diff --git a/libgralloc/framebuffer.cpp b/libgralloc/framebuffer.cpp

@@ -1064,6 +1066,7 @@ int mapFrameBufferLocked(struct private_module_t* module)

     info.bits_per_pixel = 16;

     info.grayscale = 0;

     info.yoffset = 0;

+     info.rotate = FB_ROTATE_CCW;

#endif

     uint32_t flags = PAGE_FLIP;

Labels (2)
0 Replies