Hello Sir,
I now get a Rev C EVK board.
The conflict message during boot disappears.
With the same kernel (ADB is configured), the mmc still does not work.
Here is my menuconfig of mmc in kernel:
--- MMC/SD/SDIO card support
[*] MMC debugging
[ ] Allow unsafe resume (DANGEROUS)
[ ] MMC embedded SDIO device support (EXPERIMENTAL)
[*] Enable paranoid SD card initialization (EXPERIMENTAL)
*** MMC/SD/SDIO Card Drivers ***
<*> MMC block device driver
[*] Use bounce buffer for simple hosts
[*] Check card status on resume
< > SDIO UART/GPS class support
< > MMC host test driver
*** MMC/SD/SDIO Host Controller Drivers ***
<*> Secure Digital Host Controller Interface support
< > MMC/SD/SDIO over SPI
[ ] Freescale i.MX Secure Digital Host Controller Interface PIO mode
<*> STMP37xx/378x MMC support
Is there anything that I configure it wrong?
Thanks!
BR,
Terry