Hi Karthik,
You can use F1 fuse option for your application with LPDDR2. and follow the reference design of MCIMX6SLEVK.
http://cache.freescale.com/files/product/hardware_tools/MCIMX6SLEVK.pdf
Depending on your application you may require LDO for other peripherals like LCD,which require 2.8V for IO supply.
If your project volume is low, you can go for customized OTP programming using KITPFPGMEVME.
Regards,
Rakhesh
Hi Karthik,
If none of the pre-programmed parts work for you, then you can order the PF-Programmer board and the socketed board and program parts for the voltages you require.
Here are the relevant links:
KITPF0100EPEVBE Product Summary Page
KITPF0100SKTEVBE Product Summary Page
The F2 sequence has SW3 output at 1.2V if that will work for you.
Regards,
Anand
Hi Yongcai Huang,
Thanks for your reply. As you said, I hope 1.5 to 1.2 V LDO might be an appealing solution.
But Freescale should deliver PMIC customized for LPDDR2 as well in future.
Hi, Karthik
Please ask FAEs/PMIC experts first, maybe there is already solution of customized PMIC OCOTP. The additional LDO is only a back up plan, as it will bring power/cost penalty.
Hi, Karthik
From the fuse description of MMPF0100, the F1 and F0's differences are not just the DDR power rails' voltage difference, it also has many other differences. So, I think programming the OTP of PMIC to F1 is not proper, one solution came to my mind is, maybe you can contact PMIC's expert to see whether there is any way to just change the DDR power rails' voltage based on the F0's OCOTP setting. If not, then maybe you can consider adding hardware circuit to scale the DDR voltage from 1.5V to 1.2V based on F0's OCOTP setting, but it will bring in some power waste. So, I think you should contact the FAEs/PMIC's expert about the possibility of customizing OCOTP setting.