MMPF0100 PMIC boost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMPF0100 PMIC boost

1,418件の閲覧回数
legbam5
Contributor I

I want to use the boost Regulator to generate a voltage higher than 5 V. It should be near by 7 V. How to handle the feed back way by a resistor devider and what is with the Maximum Rating of the SWBSTLX?

0 件の賞賛
返信
1 返信

1,273件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

I’m afraid it is not possible to generate a voltage greater than 5.150V out of the Boost regulator embedded in the MMPF0100 codec.

My recommendation would be to use an external 7.0V boost regulator in order to get this voltage.


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信