MIPI CSI-2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIPI CSI-2

1,582 Views
kapilkumar
Contributor III

Hello Friends

I am just trying to interface camera cmos sensor module through i.mx6 processor. How do i achieve data synchronization, and what will be the maximum clock provided to camera module through ADV7281-M.

Regards,

Kapil

0 Kudos
Reply
1 Reply

1,484 Views
igorpadykov
NXP Employee
NXP Employee

Hi Kapil

i.MX6 MIPI CSI-2 supports up to 1 Gbps speed

1.jpg

steps for supporting new camera are given on

Some Experience When Enable MIPI Camera

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply