MIMXRT1176AVM8A UART Debug pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1176AVM8A UART Debug pins

ソリューションへジャンプ
695件の閲覧回数
eRgnmrt
Contributor III

Hello,which UART ports are used for debugging i.MX RT1170 

 

Thanks & Regards,

0 件の賞賛
返信
1 解決策
633件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @eRgnmrt 

I hope you are doing well.

I understand as debug pins , the default pins that our MCUXpresso SDK examples use to output PRINTF() messages. If I did not understood well, please, let me know. 

Those pins are GPIO_AD_24 and  GPIO_AD_25. For more details refer to the Reference manual or schematic of our RT1170-EVK. Below an snapshot from the RM. 

diego_charles_0-1692037409625.png

All the best, 

Diego

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
609件の閲覧回数
eRgnmrt
Contributor III

hi @diego_charles thank you 

634件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @eRgnmrt 

I hope you are doing well.

I understand as debug pins , the default pins that our MCUXpresso SDK examples use to output PRINTF() messages. If I did not understood well, please, let me know. 

Those pins are GPIO_AD_24 and  GPIO_AD_25. For more details refer to the Reference manual or schematic of our RT1170-EVK. Below an snapshot from the RM. 

diego_charles_0-1692037409625.png

All the best, 

Diego

 

 

0 件の賞賛
返信