MIMXRT1064 EVK I2S Data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1064 EVK I2S Data

1,407 Views
nanjun
Contributor III

Hello,

the SAI interrupt playback example utilizes 16 bits per frame to sample audio data from microphone with a fs of 16k. the codec WM8960 was used here. The data in Buffer is shown 40,0; 41,0;  244,255, 251,255; 12,0; 251,255;249,255 ... when I ran this example in a office environment.  Attached is a screen shoot of the Buffer.

I did not do any modification of the original code. But the values are quite different from frame to frame. What do they mean? Should they be similar when the noise level stays at a relatively same level?

Thanks in advance.

Kind regards,

Nanjun

0 Kudos
Reply
0 Replies