MIMXRT1062 USB Host Bootloader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1062 USB Host Bootloader

1,041件の閲覧回数
tbonkers
Contributor III

I need an USB host bootloader for my project; the idea is to perform firmware update in the field by connecting an  USB pen drive.

Is there a reference application showing similar functionality?

0 件の賞賛
返信
1 返信

1,008件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @tbonkers ,

 

Actually so far we just have a Host MSD demo for reference, usb_host_msd_fatfs, you may use it as a starting point for usb host bootloader application.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信