MIMXRT106|| Audio/ Speaker Connection/ Audio processing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT106|| Audio/ Speaker Connection/ Audio processing

3,498件の閲覧回数
goyal9076
Contributor I

Hi,

I am facing problem in interfacing speaker. Till now I have understand that MQS pin are used for that. Is there any other provision other than this?

Also need to have a block diagram for audio processing if I/P is provided at SAI3 pins through I2S communication. 

0 件の賞賛
返信
3 返答(返信)

3,489件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello

Hope you are well.
Yes, you can use the MQS to interface a speaker but you will need external circuitry since the output is a PWM signal.

This post might be helpful since it refers to the circuit to connect the speaker as well as an example code: https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070

You can also connect a speaker through an external audio codec like WM8960 that is on our boards. The example codes can be found at the SDK.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信

3,476件の閲覧回数
goyal9076
Contributor I

Hi,
Are you recommending attached image for MQS driver circuitry?

Q1- In this circuitry, Is Power AMP required in between buffer and audio jack?

Q2- Attaching the image of our schematic dig for the implementation of speaker connection, Can you please confirm whether it will work or not? If any modification required, please comment.

Also please share the test code and drivers needed.

0 件の賞賛
返信

3,438件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Yes, the circuit attached from my colleague can be helpful. With the 74vc244 you won´t need an RC circuit.

A1 - No, the parts in that circuitry are enough to reproduce music.

A2 - Your schematic looks fine. We have to consider that the output from MQS is a PWM signal so we first need to add an RC filter and improve the signal with an amplifier.
The example was uploaded by Kerry in this post:  https://community.nxp.com/t5/i-MX-Processors/RT1064-MQS-Driver-Circuitary/m-p/1348070
For the drivers you need to install the SDK: https://mcuxpresso.nxp.com/en/welcome

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 件の賞賛
返信