MIMXRT1050-EVK OCRAM single step debugging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1050-EVK OCRAM single step debugging

1,614件の閲覧回数
michaelwhite
Fresh Out Contributor

Hi,

I have a MIMXRT1050-EVK (not EVKB) and am running the 2.3.0 SDK with LWIP and FreeRTOS and developing with MCUXpresso IDE.  My application is too large to fit into ITC RAM so it is placed in OC RAM.  If I load the application and attempt to single step (step into or step over), nothing happens to the M7 registers except the cycle register increases by 11 - the program does not step forward, the PC does not change, etc...  If I place a breakpoint further along in the code then "Resume" the code, the application hits the breakpoint; however, single stepping from the breakpoint again results in no change to the PC.

If I completely disable OCRAM caching (TypeExtField = 0, IsShareable = 0, IsCacheable = 0, IsBufferable = 0) then I can single step.  Unfortunately, with OCRAM  caching disabled the application does not appear to be fast enough to handle high speed USB while running FreeRTOS - interrupts are dumped to the queue faster than the application can service them.  I have tried both Write Through (IsCacheable = 1, IsBufferable = 0) and Write Back (IsCacheable = 1, IsBufferable = 1) caching; neither allow me to single step in OCRAM.

This problem occurs with both the on-board debugger and an external Keil Ulink2 debugger, so I do not think it is a debugger issue.

Likewise, I do not think this is an MCUExpresso issue as I am able to single step with caching off or when the executable is in ITC.

Is there a way to single step the debugger with OCRAM cache enabled?

Thanks!

タグ(2)
0 件の賞賛
返信
1 返信

1,474件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  perhaps the following helps.

https://community.nxp.com/message/985705 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信