MIMX8ML8CVNKZAB Thermal Management

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIMX8ML8CVNKZAB Thermal Management

1,853 次查看
Pavanecon
Contributor II

Hi Team,

We developed a customized board for our application with MIMX8ML8CVNKZAB SOC. During our thermal test, we observed that at 55 °C, our board is getting shutdown. This is due to the default thermal shutdown at 95 °C junction temperature.

As per the reference manual, the SOC Thermal Shutdown temperature can be configured up to 105C.

Now we are planning to configure the thermal shutdown temperature to 100 °C.

So, is it worth changing the thermal shutdown temperature to 100 °C? or do we have any risk of doing this?

Can NXP provide any views or comments on this?

标签 (1)
0 项奖励
回复
3 回复数

1,790 次查看
Pavanecon
Contributor II

Hi Joanxie,

Thanks for the reply

0 项奖励
回复

1,826 次查看
Pavanecon
Contributor II
Is it safe to change the thermal shutdown temperature to 100 C? Can anyone reply on this
0 项奖励
回复

1,820 次查看
joanxie
NXP TechSupport
NXP TechSupport

refer to the data sheet, industrial can support up to the 105

joanxie_0-1726708185871.png

but consider the margin 10°C to the max temperature, we suggest customer set 95°C as critical temperature, which not mean the 100 is not allowed, just consider the sensor accuracy

0 项奖励
回复