MIMRTXT106 chip variant drop in replacement?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMRTXT106 chip variant drop in replacement?

980 Views
biomurph
Contributor I

I'm working on a project that originally calls for the MIMXRT1062DVL6B and this particular variant in the 106x family is not in stock any time soon.

I do see some parts in this 106x family that are in stock. In looking at the data sheet I see many variant part numbers of this chip. One has voice control capability and another has face recognition capability. 

The one that I mention above is the 1062, which is "Full Feature", and there is also a 1061, which is "Standard Feature".

My question is, what is the actual difference in these variants? Would I be able to use the 106L, 106F, or 1061 as a drop in replacement for the 1062? I am having a hard time telling the difference between the Full Feature and Standard Feature variants. 

It seems like the "L" and "F" variants are the same as the "2", just with firmware flashed by the manufacturer. Can I use it and overwrite the RTOS and other stuff with my own?

Thanks for your consideration

Labels (1)
0 Kudos
Reply
0 Replies