MFGTools

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGTools

21,210件の閲覧回数
kapilkumar
Contributor III

Hello

what changes i have to make in MFGTools2 if i want to burn my own images ? I am refering the Documents that comes along with the this tools.

I have u-boot.bin and uImage. I just want to know where to keep these two files in MFGTools Directory so that i can bring up u-boot and kernel on my sabre-sd platform. Any other changes if i have to make ,please guide me .

ラベル(3)
11 返答(返信)

16,923件の閲覧回数
vijaikumar
Contributor III

Hello Kapil,

                I am quickly summarizing the required steps to support custom board in MFGTOOL. Do let me know if you want more information.

1. Update firmware files for MFGTool

2. Update final images to be flashed

3. Modify UCL script file (If needed)

4. Modify .vbs file (if needed)

First you need to copy the u-boot zImage device tree built for MFGTool into the following location

Profiles\Linux\OS Firmware\firmware

Next, You need to copy the images which you wish to flash in your board into the following location

Profiles\Linux\OS Firmware\files

Modify UCL script if you are using different file name other than what is mentioned in UCL.xml file. For example if your file name is kapil-uboot.imx then change the UCL script as folllows

<CMD state="Updater" type="push" body="send" file="files/kapil-uboot.imx" ifdev="MX6Q">Sending u-boot.bin</CMD>

Modify VB script(mfgtool2-yocto-mx6-sabresd-sd). Update the mmc number, if required.

Set wshShell = CreateObject("WScript.shell")

wshShell.run "mfgtool2.exe -c ""linux"" -l ""SDCard"" -s ""board=sabresd"" -s ""mmc=1"" "

Set wshShell = Nothing

Now you can run the .vbs file to start flashing your images to target.

0 件の賞賛
返信

16,923件の閲覧回数
saurabh206
Senior Contributor III

Hello Kapil

You need to keep those file in

mfgtool\Profiles\MX6Q Linux Update\OS Firmware\files  -> for Linux BSP

Following files are important for your custom board and new profile creation.

You need to create your profile in UCL.xml

mfgtool\Profiles\MX6Q Linux Update\OS Firmware\UCL.xml

like

<LIST name="ubuntu-SabreSD-eMMC" desc="Choose eMMC android as media">

Select this profile in cfg.ini file.

mfgtool\cfg.ini

name = ubuntu-SabreSD-eMMC

Thanks

Saurabh

0 件の賞賛
返信

16,923件の閲覧回数
kapilkumar
Contributor III

Hello Saurabh

Suppose i have kapil-u-boot.bin file (for U-Boot). I added into

*mfgtool\Profiles\MX6Q

Linux Update\OS Firmware\files\kapil-u-boot.bin. *

Is there anything i need to delete before loading into sd-card because

there is already a file* "u-boot-mx6dl.bin" in the path mfgtool\Profiles\MX6Q

Linux Update\OS Firmware\files ???*

I tried loading into sd-card by deleting* "u-boot-mx6dl.bin", *then, it is

not getting downloaded and am getting an error window saying*

"initialization operation failed".*

Please, help me.

Best Regards,

Kapil Kumar.

On Thu, Dec 31, 2015 at 11:08 AM, saurabh206 <[email protected]>

0 件の賞賛
返信

16,923件の閲覧回数
saurabh206
Senior Contributor III

Hello Kapil,

Are you getting error during firmware update time?  Does firmware update done correctly?

Or During boot up time you are getting error?

0 件の賞賛
返信

16,923件の閲覧回数
kapilkumar
Contributor III

Hi Saurabh

I am getting error during Firmware updation time.

On Thu, Dec 31, 2015 at 4:37 PM, saurabh206 <[email protected]>

0 件の賞賛
返信

16,923件の閲覧回数
saurabh206
Senior Contributor III

Hi Kapil,

You can check error log in mfgtool\MfgTool.log

also what error message display on console?

0 件の賞賛
返信

16,923件の閲覧回数
kapilkumar
Contributor III

Hi Saurabh

Please find an attachment. i just let you know what i did till now and what

error log i am getting.

if anything other , i have to do ,please let me know.

Thanks

Kapil Kumar

On Fri, Jan 1, 2016 at 11:12 AM, saurabh206 <[email protected]>

0 件の賞賛
返信

16,923件の閲覧回数
saurabh206
Senior Contributor III

Hello Kapil

Your first step is wrong, Firmware binary used to boot the board in firmware update mode.

In 2nd step,

You need to put your binary in files folder.

Do modification for updated binary after following code in your ucl.xml profile.

"<CMD state="BootStrap" type="jump" > Jumping to OS image. </CMD>"

Please make sure that your modified UCL.xml profile used in cfg.ini file.

Have you modified your cfg.ini file ?

Which board you are using?

which BSP you are using?

0 件の賞賛
返信

16,923件の閲覧回数
kapilkumar
Contributor III

Hi Saurabh

Please find an attachment. I am working on SABRE-SD Platform

and using Android BSP.

On Fri, Jan 1, 2016 at 1:29 PM, saurabh206 <[email protected]>

0 件の賞賛
返信

16,923件の閲覧回数
saurabh206
Senior Contributor III

Hi Kapil

For Android BSP you need build boot.img.

Also make sure that you have used right profile according to your board.

You have used profile for i.MX6solo/DL board, I think this is wrong according to your SABRE SD board.

0 件の賞賛
返信

16,921件の閲覧回数
kapilkumar
Contributor III

Hi Saurabh

I need boot.img for Android BSP. Okay..then, where i will place the

boot.img, means in which folder of MFGTools??? But Saurabh, boot.img is

also a kernel image file and uImage is also a kernel image file . so ,

both is needed to be there in the MFGTools???

One more question:

see, i have a folder "android" which contain images shown below:Path of

android folder is

*Mfgtools-Rel-13.01.00_ER_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS

Firmware\files\android *

these five images is not mine. these images came alongwith the MFGTool

*So , the question is to make it sure from yourside also that i have to

keep ( kapil-u-boot.bin, boot.img, uImage) in files folder or android

folder...*

*shall i need to remove u-boot-6dl.bin and boot.img with our

kapil-u-boot.bin and boot.img files respectively from the android

folder????*

Thanks Saurabh for helping me with the long time.

On Fri, Jan 1, 2016 at 5:21 PM, saurabh206 <[email protected]>

0 件の賞賛
返信