MFGTool Updater Error 0x500

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFGTool Updater Error 0x500

1,009件の閲覧回数
yuanming
Contributor I

On a windows 7 machine, I am trying to use MFGTool to download a Linux profile (i.e. MX28 Linux Update) via USB to a TX28-4031 development board. The output option was set to "Singlechip NAND". But when I clicked "Start", it would eventually fail with the following error message:

"Updater Error 0x500 (1280) - The current thread has already been converted to a fiber".

If the output option is set to SD (with uboot) or SD (without uboot), the writing will be successful.

Any thoughts on how to fix the issue with "Singlechip NAND" as an output option? Thanks for your kind help in advance!

0 件の賞賛
返信
0 返答(返信)