MFGTool Updater Error 0x500

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGTool Updater Error 0x500

994 Views
yuanming
Contributor I

On a windows 7 machine, I am trying to use MFGTool to download a Linux profile (i.e. MX28 Linux Update) via USB to a TX28-4031 development board. The output option was set to "Singlechip NAND". But when I clicked "Start", it would eventually fail with the following error message:

"Updater Error 0x500 (1280) - The current thread has already been converted to a fiber".

If the output option is set to SD (with uboot) or SD (without uboot), the writing will be successful.

Any thoughts on how to fix the issue with "Singlechip NAND" as an output option? Thanks for your kind help in advance!

0 Kudos
Reply
0 Replies