MFG Tools: eMMC partitioning for Android

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFG Tools: eMMC partitioning for Android

16,127件の閲覧回数
carlobarbaro
Contributor III

Hello,

I'm studing the process performed by MFG Tools to partition, format and installing the Android firmware on a eMMC device.

Looking at the mksdcard-android.sh script, I see the following:

# call sfdisk to create partition table

# get total card size

seprate=40

total_size=`sfdisk -s ${node}`

total_size=`expr ${total_size} / 1024`

boot_rom_sizeb=`expr ${BOOT_ROM_SIZE} + ${BOOTLOAD_RESERVE}`

extend_size=`expr ${SYSTEM_ROM_SIZE} + ${CACHE_SIZE} + ${VENDER_SIZE} + ${MISC_SIZE} + ${seprate}`

data_size=`expr ${total_size} - ${boot_rom_sizeb} - ${RECOVERY_ROM_SIZE} - ${extend_size} + ${seprate}`

# destroy the partition table

dd if=/dev/zero of=${node} bs=1024 count=1

# create partitions

sfdisk --force -uM ${node} << EOF

,${boot_rom_sizeb},83

,${RECOVERY_ROM_SIZE},83

,${extend_size},5

,${data_size},83

,${SYSTEM_ROM_SIZE},83

,${CACHE_SIZE},83

,${VENDER_SIZE},83

,${MISC_SIZE},83

EOF

Can someone explain the meaning the additional ${seprate} with size of 40MB, added to both extended and data partition?

Doing this way, the partitioning exceed the total size of storage device.

This is also reported by logs generated by the target when MFG Tools are partitioning the device:

Disk /dev/mmcblk0: 238592 cylinders, 4 heads, 16 sectors/track

sfdisk: ERROR: sector 0 does not have an msdos signature

/dev/mmcblk0: unrecognized partition table type

Old situation:

No partitions found

Warning: given size (6392) exceeds max allowable size (6352)

New situation:

Units = mebibytes of 1048576 bytes, blocks of 1024 bytes, counting from 0

  Device Boot Start End MiB #blocks Id System

/dev/mmcblk0p1 0+ 15 16- 16383+ 83 Linux

/dev/mmcblk0p2 16 23 8 8192 83 Linux

/dev/mmcblk0p3 24 1103 1080 1105920 5 Extended

/dev/mmcblk0p4 1104 7495 6392 6545408 83 Linux

/dev/mmcblk0p5 24+ 535 512- 524287+ 83 Linux

/dev/mmcblk0p6 536+ 1047 512- 524287+ 83 Linux

/dev/mmcblk0p7 1048+ 1055 8- 8191+ 83 Linux

/dev/mmcblk0p8 1056+ 1063 8- 8191+ 83 Linux

Warning: partition 4 extends past end of disk

Successfully wrote the new partition table

Re-reading the partition table ...

mmcblk0: p1 p2 p3 < p5 p6 p7 p8 > p4

mmcblk0: p4 size 13090816 extends beyond EOD, truncated

タグ(3)
0 件の賞賛
返信
2 返答(返信)

3,981件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I have delved into this, but I have not found the reason of the additional ${seprate}.

But I tried to set the variable to 0 and the partitions and Android seems to be working with no issues.

Best Regards,

Alejandro

0 件の賞賛
返信

3,981件の閲覧回数
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 件の賞賛
返信