Hi ,
I used both SDCARD images from
L4.9.88_2.0.0_MX6QDLSOLOX
L4.14.98_2.0.0_MX6QDLSOLOX
and write it using Linux dd command to a 32G SDCARD .
OS: Ubuntu 18.04
No error , write was successful
But the MCIMX6SX-SDB don’t boot ( no output messages on Putty )
If I use other iMX6SX images from other sources it works .
Any idea what could go wrong ?
Best Regards
Klaus
Hi Carlos,
thank your for the fast reply , it fix my problem !
Best Regards
Klaus
Hi Klaus,
It seems it was missed flashing the proper U-Boot, as the same .sdcard file is for multiple platforms. Please refer to the procedure from the following Community thread to complete the flashing of thr U-Boot using either the dd command, or UUU tool:
Understanding imx8mqevk and booting linux from sdcard
Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------