MCIMX6S5DVM10AC processor and MMPF0100F2AEP PMIC failure

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6S5DVM10AC processor and MMPF0100F2AEP PMIC failure

1,715 Views
Amiraroslan
Contributor I

Hi, 

We have a design that uses the MCIMX6S5DVM10AC device with PMIC MMPF0100F2AEP. The design then reported a failed soft reboot (cmd reboot without plug off) and caused a freeze screen on the instrument. Hence, we would like to know: 

1) Which pin of the MCIMX6S5DVM10AC processor IC is used for reset?

2) How can we verify the reset power pulse? Do you have any reference pulse diagrams?

Thanks!

0 Kudos
Reply
4 Replies

1,694 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello; I hope you are doing well.

I suggest you check the section 60.4.1 "Reset and Power-up Flow" of reference manual to check information related to reset signals managed by the SRC module:

Jorge7u7_0-1699889006854.png

Please check a reference pulse timing diagram on datasheet:

Jorge7u7_1-1699889021666.png

Best regards.

 

0 Kudos
Reply

1,682 Views
Amiraroslan
Contributor I
Hi, thanks for your suggestions. So, which pins should I probe? 
0 Kudos
Reply

1,674 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Yes, that should be the pin to check POR_B (C11).

Best regards.

0 Kudos
Reply

1,680 Views
Amiraroslan
Contributor I
For POR our Product Engineer try on the C11 pin. But for reset, which pin should we use ya?
0 Kudos
Reply