MCIMX6Q4AVT10AC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCIMX6Q4AVT10AC

2,104 次查看
hiroshitakahash
Contributor II

(question)

Can '1GHZ' CPU be used by '800MHZ '

标签 (1)
4 回复数

1,987 次查看
AnsonHuang
NXP Employee
NXP Employee

Adding "arm_freq=800" is only working for L3.0.35, to make it work for all kernel, I think you can change the /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq to 792000. just "echo 792000 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_max_freq" after linux kernel boot up.

0 项奖励
回复

1,987 次查看
CarlChien
NXP Employee
NXP Employee

Hi Hiroshi,

If your BSP is Android or Linux, you can add "arm_freq=800" into your bootloader parameters. Lets CPU work at special frequency (MHz).

Best regards,

Carl

1,986 次查看
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Hiroshi,

If my understanding is correct, you want to run a 1GHz i.MX6 processor at 800MHz (core frequency), right? If so, the answer is yes, you just have to configure the clocks (see reference manual chapter 18) so the resulting frequency is the one you desire. If you are using an OS like Linux, this is done automatically by configuring some settings. I'm mainly focused on HW, but a SW person can help you with this.

Best regards.

Jorge.

0 项奖励
回复

1,987 次查看
Yuri
NXP Employee
NXP Employee

Why not ?

0 项奖励
回复