MCIMX6Q-SDP battery issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX6Q-SDP battery issues

1,822 Views
m_c
Senior Contributor I

The electrical discharge statuses are not same. (DC 5V off)

  a. Sometimes cannot switch to battery mode(3.7V/4.6Ah) smoothly.

  b. Sometimes device will reset automatically and into battery mode after power on.

  c. Sometimes device will continuous reboot. (The machine has been restart again and again)

We are now using 3.8V/3A*2 sets switching power to simulate battery DC 5V off, MCIMX6Q-SDP can switch to battery mode smoothly.

How to reduce the current electrical use, and switch power and battery mode smoothly.

Labels (1)
Tags (2)
0 Kudos
Reply
2 Replies

1,724 Views
jamesbone
NXP TechSupport
NXP TechSupport

Is this behavior under Linux, or Android? What BSP are you using?   Can you please share the steps to try to replicate the issue.

0 Kudos
Reply

1,724 Views
m_c
Senior Contributor I

BSP Version =android_jb4.3_1.1.0-ga_source

battery = 3.7V/4.6Ah cannot switch to battery mode

device will reset automatically or device will continuous reboot.

How to reduce the current electrical use, and switch power and battery mode smoothly.

0 Kudos
Reply