MCIMX6Q-SDP battery application issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCIMX6Q-SDP battery application issues

1,380件の閲覧回数
felixhsu
Contributor III

Hi All

Hardware: MCIMX6Q-SDP

Software: Android_JB4.3_1.1.0

Use battery power supply application issues as below,

1. Could modification battery detect voltage? if yes, How to change it.

2. What is the minimum current requirement, when the power from DC in switch to battery?

Thanks.

ラベル(6)
タグ(1)
0 件の賞賛
返信
1 返信

1,235件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Felix,

>>1. Could modification battery detect voltage? if yes, How to change it.

On SabreSDP board, 2 MAX8903C chargers was used, the chager IC can only charge battery with 4.2V full voltage, so voltage that needs to be detected should be max 4.2V, if you are using Li battery with 3.6V, you don't need to do any modification.

>>2. What is the minimum current requirement, when the power from DC in switch to battery?

At differenct charging stage, Charging current is different, it is determined by charger IC, so you had better read MAX8903C datasheet carefully.


Have a great day,
TIC  Weidong

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信