Dear jimmychan ,
You are right... :smileyhappy: I was using BSP 11.09... So i downloaded 11.05 and compiled it.
It went well. But theres another problem here while compiling SSI ( sound ) driver ( in MXC Support Drivers-> MXC SSI Support-> SSI Support) ..
I need audio badly.. Or can u suggest any other driver ?? I'm working on SABRE tablet..
Here is last few lines of output...
make[1]: `include/generated/mach-types.h' is up to date.
CALL scripts/checksyscalls.sh
CHK include/generated/compile.h
GZIP kernel/config_data.gz
IKCFG kernel/config_data.h
CC kernel/configs.o
LD kernel/built-in.o
CC drivers/mxc/ssi/ssi.o
CC drivers/mxc/vpu/mxc_vpu.o
CC drivers/mxc/vpu/mxc_vl2cc.o
drivers/mxc/ssi/ssi.c: In function 'get_ssi_fifo_addr':
drivers/mxc/ssi/ssi.c:111: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'get_ssi_base_addr':
drivers/mxc/ssi/ssi.c:128: error: dereferencing pointer to incomplete type
drivers/mxc/ssi/ssi.c: In function 'ssi_rx_fifo_counter':
drivers/mxc/ssi/ssi.c:568: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:572: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c: In function 'ssi_tx_fifo_counter':
drivers/mxc/ssi/ssi.c:939: warning: overflow in implicit constant conversion
drivers/mxc/ssi/ssi.c:943: warning: overflow in implicit constant conversion
make[3]: *** [drivers/mxc/ssi/ssi.o] Error 1
make[2]: *** [drivers/mxc/ssi] Error 2
make[2]: *** Waiting for unfinished jobs....
CC drivers/video/logo/logo_linux_mono.o
CC drivers/video/logo/logo.o
LD drivers/video/logo/built-in.o
LD drivers/video/built-in.o
LD drivers/mxc/vpu/vpu.o
LD drivers/mxc/vpu/built-in.o
make[1]: *** [drivers/mxc] Error 2
make: *** [drivers] Error 2
error: Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
RPM build errors:
Bad exit status from /home/wintu/ltib/tmp/rpm-tmp.30321 (%build)
Build time for kernel-2.6.35: 4316 seconds
Failed building kernel-2.6.35
f_buildrpms() returned an error, exiting
traceback:
main:560
Started: Tue Jan 15 05:07:36 2013
Ended: Tue Jan 15 06:19:33 2013
Elapsed: 4317 seconds
These packages failed to build:
kernel-2.6.35
Build Failed
Exiting on error or interrupt
I get error regarding dereferenced pointer. Could you please check it out. ..