MC34708VM question...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC34708VM question...

1,393 Views
changliu
Contributor I

Dear experts,

Based on MC34708VM datasheet and errata, charger and coulomb counter features are removed. Under Pin description, E6, F6 and E8 are indicated as "NC". However, in our current design in production, these three pins are pulled to High state permanently (3.6V). Is it ok to do this? or are they absolutely needed to be "NC"?

Regards,

LC

1 Reply

1,291 Views
reyes
NXP TechSupport
NXP TechSupport

Hi LC,

Since the Coulomb Counter on the MC34708 is no longer supported, then yes, the recommendation is to leave the mentioned pins as NC, however, if in your design these pins are already connected, then you can leave then connected permanently to 3.6V without any problem.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------