MC33PF8200DEES

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
837件の閲覧回数
Chethanbg
Contributor III

We are using device MC33PF8200DEES in our custom design with MiMX8DX6AVLFZAC processor.

PMIC says input voltage range 2.5V to 5.5V .Our custom board gives 3.3V input to PMIC but can we get 3.3V output in SW7(Buck 7 configured as 3.3V output)?

There is no graph or formula in MC33PF8200DEES datasheet about output voltage with respect to input voltage how much it can drop max from input?

Please clarify.

 

0 件の賞賛
返信
1 解決策
741件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No formular here,because of lack of maximum duty cycle parameter, but according the maximum current 4.5A and high side MOSFET RDSon 0.15ohm, the estimate maximum output value up to 2.6 or 2.7V @VIN3.3V

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
805件の閲覧回数
Chethanbg
Contributor III

what will be the output then how much will it drop?Any formula is there?

What is the minimum input voltage need to give to get output as 3.3V?

0 件の賞賛
返信
742件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No formular here,because of lack of maximum duty cycle parameter, but according the maximum current 4.5A and high side MOSFET RDSon 0.15ohm, the estimate maximum output value up to 2.6 or 2.7V @VIN3.3V

0 件の賞賛
返信
834件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

No,if the input is 3.3V the output can't get 3.3V.

 

0 件の賞賛
返信