MC33PF8200DEES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33PF8200DEES

Jump to solution
836 Views
Chethanbg
Contributor III

We are using device MC33PF8200DEES in our custom design with MiMX8DX6AVLFZAC processor.

PMIC says input voltage range 2.5V to 5.5V .Our custom board gives 3.3V input to PMIC but can we get 3.3V output in SW7(Buck 7 configured as 3.3V output)?

There is no graph or formula in MC33PF8200DEES datasheet about output voltage with respect to input voltage how much it can drop max from input?

Please clarify.

 

0 Kudos
Reply
1 Solution
740 Views
guoweisun
NXP TechSupport
NXP TechSupport

No formular here,because of lack of maximum duty cycle parameter, but according the maximum current 4.5A and high side MOSFET RDSon 0.15ohm, the estimate maximum output value up to 2.6 or 2.7V @VIN3.3V

View solution in original post

0 Kudos
Reply
3 Replies
804 Views
Chethanbg
Contributor III

what will be the output then how much will it drop?Any formula is there?

What is the minimum input voltage need to give to get output as 3.3V?

0 Kudos
Reply
741 Views
guoweisun
NXP TechSupport
NXP TechSupport

No formular here,because of lack of maximum duty cycle parameter, but according the maximum current 4.5A and high side MOSFET RDSon 0.15ohm, the estimate maximum output value up to 2.6 or 2.7V @VIN3.3V

0 Kudos
Reply
833 Views
guoweisun
NXP TechSupport
NXP TechSupport

No,if the input is 3.3V the output can't get 3.3V.

 

0 Kudos
Reply