Low Speed eCSPI Port on iMX6SX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Low Speed eCSPI Port on iMX6SX

1,462件の閲覧回数
damonkutten
Contributor II


Hello,

  In the IMX6SXRM document (page 176) it states that there are "Four eCSPI (Enhanced CSPI), three of them can support up to 52 Mbps, one can be of low speed". But the low speed eCSPI port is not identified anywhere. Which eCSPI port is low speed on this device, and what is its actual speed?

0 件の賞賛
返信
1 返信

1,340件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Damon

all i.MX6SX eCSPI modules are identical, so this is inaccuracy

in description.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信