Low Speed eCSPI Port on iMX6SX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Low Speed eCSPI Port on iMX6SX

1,458 次查看
damonkutten
Contributor II


Hello,

  In the IMX6SXRM document (page 176) it states that there are "Four eCSPI (Enhanced CSPI), three of them can support up to 52 Mbps, one can be of low speed". But the low speed eCSPI port is not identified anywhere. Which eCSPI port is low speed on this device, and what is its actual speed?

0 项奖励
回复
1 回复

1,336 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Damon

all i.MX6SX eCSPI modules are identical, so this is inaccuracy

in description.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复