Loopback for RGMII MAC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loopback for RGMII MAC

5,648 Views
niteshsahay
Contributor III

Hi

I am using iMX6 Quad core processor and MAC signals for RGMII interface coming out from processor can be externally loopback and tested?

Labels (1)
2 Replies

4,913 Views
RossMcLuckie
NXP Employee
NXP Employee

Hi,

This is very dependent on what you are trying to achieve here.

If to test your hardware (PCB) then likely the most effective way to do this is create a loopback ethernet cable and plug this into your RJ-45 connector during test, this way you are testing from the processor all the way out to the RJ-45 connector, via the PHY.

You can google ethernet loopback for further information on this.

Another option would be to look at the PHY you plan to use for loopback modes, this would allow you to test from the processor to PHY connections, but may not cover the PHY to RJ-45 connections.

Within the ENET controller I see no RGMII loopback modes within the documentation, there appears to be RMII and MII loopback modes, but I think they will provide very little benefit if they only test the controller on the processor and provide no real hardware testing.

If you still have a reason for wanting to test the RGMII pin connectivity only, you could use the GPIO mode of these pins and write a small test for this, but again not sure this actually achieves a lot for you, depending on your exact needs.

Regards

Ross

4,913 Views
roya_azimi93
Contributor II

Hi, 

it was my question, too. I don't want using phy . is it possible to loopback mac pins? like this:

RX0 -- > TX0. 

.

.

RX3 --> TX3.

RX_CLK --> TX_CLK

RX_DV --> TX_DV.

0 Kudos
Reply