Load current of GPIO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Load current of GPIO

1,355 次查看
KrishnaPrasad1z
Contributor I

Hi,

We are using i.Mx6UL based custom board.
We need withstand load current of GPIO pin for appropriate LED selection(Considering GPIO voltage as 3.3V).
I could not find this detail in the datasheet. Please provide the detail on this.

Thanks in advance.

Regards,
Krishna

标签 (1)
0 项奖励
回复
1 回复

1,249 次查看
b36401
NXP Employee
NXP Employee

Actually GPIO buffer load capacity is not specified in units of current.
It is only specified in terms of buffer drive strength or output impedance.
You can refer chapter 4.8.1 "Single Voltage GPIO Output Buffer Impedance" of i.MX 6UltraLite DataSheet.

And you can use IBIS models to estimate the current.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复