Linux system clock when iMX6 is in deepsleep

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux system clock when iMX6 is in deepsleep

1,786件の閲覧回数
sivaraj
Contributor II

Hi,

I am using iMX6 processor with Linux OS in a project. Can you please let me know whether linux system clock will be running when the iMX6 is in deepsleep mode? If it will not be running, how the system clock will be updated in when the iMX6 wakes up.

Thanks,

Sivaraj

0 件の賞賛
返信
2 返答(返信)

1,734件の閲覧回数
sivaraj
Contributor II

Hi,

Thanks for the reply.

I am trying to understand how the linux system clock works in the deepsleep mode of iMX6 processor. I could not get the answer from the documents.

Can you please help me understand?

Thanks,

0 件の賞賛
返信

1,734件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sivaraj,

Deep sleep mode is implemented in linux, please check 
Chapter 21 Low-level Power Management (PM) Driver of the  Linux Manual for description of Mem (suspend to RAM) mode and AN4509 i.MX 6Dual/6Quad Power Consumption Measurement sect. Deep Sleep Mode
https://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf
Note, if custom modifications of linux sources are needed, may be recommended
to apply to profesional services or elevate request through local fae channel (project info
may be needed).

Regards

0 件の賞賛
返信