Linux, imx6q SPI as slave

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Linux, imx6q SPI as slave

5,143 次查看
angelo_d
Senior Contributor I

Dear all,

i have actually a MCU connected to imx6q, in the classic MISO->MISO, MOSI->MOSI. Actually Linux is master and MCU is salve. All works fine. I would try, and as far as i know, with same wiring it should be possible, an inversion of role. Linux slave and MCU master. About MCU side thing is simple.  About linux seems slave mode is not supported. Is this possible ? I found also a possible patch:

[v2,8/8] spi: imx: Add support for SPI Slave mode for imx53 and imx6 chips - Patchwork 

Any help to have imx6q as SPI configured as slave is appreciated.

Regards,

angelo

标签 (1)
0 项奖励
回复
6 回复数

3,907 次查看
fabio_estevam
NXP Employee
NXP Employee

Hi Angelo,

mx6 slave driver support has been accepted recently:

https://git.kernel.org/pub/scm/linux/kernel/git/next/linux-next.git/commit/drivers/spi/spi-imx.c?h=n... 

Can you try linux-next tree, that has this support in place?

Regards,

Fabio Estevam

0 项奖励
回复

3,907 次查看
afeionline
Contributor I

The link is failure,could you attach a new link please?

0 项奖励
回复

3,907 次查看
fabio_estevam
NXP Employee
NXP Employee
0 项奖励
回复

3,907 次查看
afeionline
Contributor I

thx!

0 项奖励
回复

3,907 次查看
angelo_d
Senior Contributor I

Hi Igor,

thanks for the support.

I implemented a minimal spi-slave linux driver, it works fine. But there is something that is not clear from the errata and that maybe you can clarify.

I have IMX6QP6AVT1AA-SBAQ1636 (for mask reference).

1) In the errata, and RM datasheet as well, it is said that for slave mode, SS_CTL bit must be set to 0 (no input chip select considered) and to always set BURST_LENGTH.

By the way, if from master side i fully disable CS and just set BURST_LENGTH on imx6q rx side, i can't get any rx interrupt happening. CS must anyway be generated at least as start of transfer, seems.

2) So, from1, if i keep master side toggling CS, it selects and de-select CS for each byte. In this new scenario i cannot in any way use BURST_LENGTH to have an interrupt for multiple bytes, seems the limit is the CS deselecting (going up) so max 1 byte actually.

These 2 points above are someway confusing me, i thought i could read i.e. a burst of 160 bit (20 bytes) without any care on CS. But seems not.

Every clarification is welcome.

Thanks,

Angelo

0 项奖励
回复

3,907 次查看
igorpadykov
NXP Employee
NXP Employee

Hi angelo

one can consider ecspi errata

https://www.nxp.com/docs/en/errata/IMX6DQCE.pdf 

and try patches on

http://lists.infradead.org/pipermail/linux-arm-kernel/2017-April/501262.html 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复