Linux Watch Dog Interrupt -i.MX6 Sabre SDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux Watch Dog Interrupt -i.MX6 Sabre SDB

1,835件の閲覧回数
sujithvarghese
Contributor I

Hello,

We try to Open WatchDog on Linux Application. Our platform is i.MX6 Sabre SDB and Linux kernel version is 3.0.5

Code Snippet "fd = open(/dev/watchdog,O_RDWR)". Linux rebooted after 60 Sec, Hope this is the default time period of WatchDog Timer.

But after reboot, the bootloader shown the previous reset status as Power - On Reset, instead of WDOG reset.

Can you please check this issue..Why it previous reset status become Power on Reset

ラベル(1)
0 件の賞賛
返信
1 返信

1,329件の閲覧回数
Yuri
NXP Employee
NXP Employee

   On the i.MX6 SDP / SDB board the i.MX6 WDOG_B pad output is connected so,

that its assertion causes (externally) POR_B.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信